Part Number: TXU0304-Q1
Other Parts Discussed in Thread: TXU0304, TXB0104, , TXB0104-Q1
Tool/software:
Hello,
we would like to connect a single master on a single SPI bus to multiple devices as represented in the image below. Only one TXU0304 will be enabled at a time using the OE pin.
Among the devices that we are looking to, there is the TXB0104-Q1 and the datasheet states that: "For proper operation, the device driving the data I/Os of the TXB0104 must have drive strength of at least ±2mA", is there any similar indication for TXU0304-Q1?
Is this configuration possible current-wise if we consider to have up to 20 TXU0304-Q1 on the same bus? The master's GPIO should be able to provide up to 20mA.
Can you confirm that there is no conflict on MISO signal when only one TXU0304-Q1 is enabled?

Many thanks