Part Number: SN74LV14A
Other Parts Discussed in Thread: SN74LV86A, SN74HCS244
Tool/software:

Are both of the two combinations shown in the diagram above OK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LV14A
Other Parts Discussed in Thread: SN74LV86A, SN74HCS244
Tool/software:

Are both of the two combinations shown in the diagram above OK?
Even so, the Vcc of the LV14A should not be 5V, right?(Although it may work with real ability)
Even if the Hi level is almost 5V, the HCS244 cannot be received, right?
Input pins on the LV14A are overvoltage tolerant, so they can receive 5V inputs from the HCS244 with no issue.

Sorry, my question is this combination.
Vcc can be 3.3V or 5V, but only one of them. (Because the board is common)
HCS inputs are not overvoltage tolerant, so the connection from the SN74LV86A will not work.
If both devices are 5V VCC, this application is fine. If a device's recommended operating conditions state 0 to VCC, the input voltage to that device must not exceed VCC or you risk damaging the device.

If the VOH of the SN74LS86 is 2.4V and the VT+ of the SN74HCS244 is 3.15V, is the SN74HCS244 not recognized as hi?
When VCC is 5V, is the maximum value of VT+ 3.5V?