Other Parts Discussed in Thread: SN74LVC1G17-Q1, SN74LVC1G125-Q1
Tool/software:
Hi Team,
I had tested the non inverting open drain buffer SN74LVC1G07QDBVRQ1 with 10K pull up resistor connected to 3.3V and 3.3V supply given to VCC.
Applied 1MHZ square wave form to input (A pin) and observed that waveform at output (Y pin) is not same as input square wave form.
As per datasheet the buffer supports up to 100MHZ frequency.
I copied tested waveform below
Can you please explain why this SN74LVC1G07QDBVRQ1 buffer behaving like above?
Also, confirm that these buffers can be used for SPI interface which operated at 33MHz.
Regards,
Srinivasu