Other Parts Discussed in Thread: TXS0108E
My customer is asking the following question:
I have a question on the specifications for the Texas instruments TXS0108E component.
The part is being used with 3.3V on the VCCA rail and 5V on the VCCB rail. My issue is with the recommended input and output voltage levels. According to the datasheet the following levels are recommended:
A side (3.3V side)
Min Max
Vih Vcci-0.2 = 3.3V-.2 = 2.9V Vcci = 3.3v
Vil 0V 0.15v
Voh Vcca * 0.67 = 3.3v * 0.67 = 2.21V
Vol 0.55V
B side (5V side)
Vih Vcci-.4V = 5V - .4 = 4.6V 5V
Vil 0V 0.15V
Voh Vccb – 0.67 = 4.33V
Vol 0.55V
It kind of an unusual part, so I may be misinterpreting the datasheet, but I can’t locate the problem. The input voltage level requirements for either side cannot be guaranteed by any standard logic family under their recommended load ranges.
Please take a look and see what you think.