This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC16T245: 10.1.1 Enable Times

Part Number: SN74LVC16T245

Tool/software:

Hi all,

I would like to confirm about ''10.1.1'' .The usage conditions are Vcca=3.3 V, Vccb=5 V.

It is defined as below, but where are the propagation delays (DIR to A) and (DIR to B) defined?

I saw the answer in the related E2E, but I could not understand it well.

(+) SN74LVC16T245: questions about datasheet section 10.1.1 - Logic forum - Logic - TI E2E support forums

For example, if I want to know tPZH (DIR to A), can I refer to the time below?

Best Regards,

Ryusuke