hi ,
the SN74LVC1G14 datasheet says
V
T+ (Positive-going input threshold voltage) is
MIN MAX 2.61V 3.33V
at VCC=5.5 V i wanted to know these values when VCC=5V. also i am using a controller whoes Voh(output voltage) is 2.8V(Min) and 3.3V(Max). will there be a problem when switching the inverter input from Low to High. Please respond to bharath.manogna@lnties.com ..