Part Number: CD74HC4060
Tool/software:
Hello everyone,
I am reviewing a control board circuit where the CD74HC4060 is used to enable and disable a part of the circuit after a fixed time.
With the following components:
Resistor: 78.7kΩ (RT0603BRD0778K7L)
Capacitor: 10nF (GRM2195C1H103FA01D)

Using the equation in the datasheet, I calculate a delay of approximately 14.2 seconds.
The reset pin is released via a 74HCT2G14 buffer, allowing the oscillator to start. Once pin 14 goes high, a MOSFET pulls down pin 11, stopping the oscillation.
However, when measuring the time between the reset deactivation and the output signal on pin 14, I observe around 14.8s, sometimes even up to 15s.
At low temperatures (-10°C to -25°C), the delay increases by an additional 200–300ms.
I have already estimated the impact of component tolerances and temperature coefficients (R and C), and the maximum I reach is around 14.5–14.6s.
So I’m wondering if I might be missing something—could temperature affect the internal oscillator of the 4060 more than expected? Are there any other consideration?
Also:
Does a pull-up/pull-down on pin 11 (OSC-IN) have any measurable effect on the oscillation frequency?
Are there any application notes or recommendations specific to this?
I cannot modify the design, but I can eventually adjust BOM values if necessary. I’m just trying to ensure my calculations are aligned with actual circuit behavior.
Thanks in advance for any insights.