Tool/software:
Hi team,
My customer wants to use the device to achieve the following function.
Input a falling trigger signal of 5us, the output is converted to 1ms, and the level needs to be converted from 3.3V to 5V

1. Is there a built-in OSC?
2. Can the IO change with the power supply, and is it a simple single power input? (The core power supply is the same as the IO power supply)
3. The first thing to do is to convert 5us into 1ms pulse output. Is TPLD1201 OK?
4. How to develop its functions? Please provide development tools
5. It is more appropriate to burn FW after PLD is loaded. Do you have a detailed burning process/tool?