Part Number: CD74ACT241
Tool/software:
Figures 3-2 and 3-3 contradict Table 3-1 in the datasheet for this part regarding pin 3
The Figures indicate the pin 3 nomenclature is 2Y0 (the same as pin 9).
Table 3-1 indicates the pin 3 nomenclature is 2Y3.
The absence of pin nomenclature 2Y3 in the Figures is conspicuous and implies there is no output for the buffer input 2A3 on pin 17. It also implies there are 2 outputs (pins 3 and 9, both 2Y0) associated with buffer input on pin 2 (1A0).
Please confirm the nomenclature for pin 3 (2Y0) in Figs 3-2 and 3-3 is an error and should be 2Y3 like in the Table.