Other Parts Discussed in Thread: TXB0104,
Tool/software:
I need a level shifter for GPIO lines where one side (VCCB = 5V) can be powered off while the other side (VCCA = 3.3V) is on.
The TXB0104 level shifter claims to have the Vcc isolation feature (if either VCC input is at GND, all outputs are in the high-impedance state). But it also says, VCCA must be ≤ VCCB. Therefore, it doesn't seem suitable.
TXU0204 also claims to have this Vcc isolation feature, but it doesn't mention the VCCA ≤ VCCB condition, but also doesn't say clearly if VCCB can be powered off while VCCA is on.
Could you please confirm if TXU0204 can be used in such condition?
Thank you!