Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204
Tool/software:
I need a level shifter for GPIO lines where one side (VCCB = 5V) can be powered off while the other side (VCCA = 3.3V) is on.
I have implemented TXB0104 in my design because it says in datasheet:
VCC isolation feature: if either VCC input is at GND, all outputs are in the high-impedance state.
But it also says VCCA must not exceed VCCB.
But when the VCCB is powered off, VCCA will exceed VCCB.
The question is, if it is ok to have VCCB be powered off while VCCA is on, because these two conditions (VCCA ≤ VCCB condition and VCC isolation feature) contradict each other?