Hello:
I want to use the logic IC to implement the buffer or mux function, but the most data sheeet don't clearly indicate the parameter about the data seepd or bandwidth.
How to evaluate the data speed of logic IC ?
My requirement is to run video at 148.5M Hz clock thourgh a 20 bit logic IC.
I want to use the SN74ALVCH162827 to implement the buffer and mux function. can SN74ALVCH162827 run at 148.5MHz clock ?