This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV1T126: Replacement for SN74LV1T126DCK

Part Number: SN74LV1T126
Other Parts Discussed in Thread: SN74AVC1T45

Tool/software:

We are currently considering level shifters for converting 1.8V to 3.3V signals as an alternative to the SN74LV1T126DCK. Although we initially planned to use the SN74LV1T126DCK, its input high-level threshold of 1.39V does not meet our requirements, as the minimum high-level output voltage on the input side is only 1.24V.
Would you be able to recommend an alternative device that satisfies these specifications?