Other Parts Discussed in Thread: TXS0101-Q1, , TXU0202-Q1, TXU0102-Q1
Tool/software:
I have a question about the TXS0102-Q1 (including TXS0101-Q1).
Side A is connected using open-drain configuration.
Since the input/output ports enter a high-impedance state when the power is turned off,
I am considering adding a 1kΩ pull-down resistor to side B.
In this case, I am concerned that the high-level voltage on side B may drop during normal operation (when both sides are powered on).
How should the minimum output high voltage (VOH(min)) on side B be calculated?
Is the calculation using VCCB × 0.67 correct?