This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC245A: Checking some odd wording in the datasheet

Part Number: SN74LVC245A


Tool/software:

In the SN74LVC245A Datasheet on page one it states:

* Supports Mixed-Mode Signal Operation on Ports (5-V Input/Output Voltage With 3.3-V VCC) 




Why would it say 5V OUTPUT voltage with 3.3 a supply voltage?
Or can this drive a 5V output from a 3.3 supply?