This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current sink or current source?

Hullo Designers and fixers !

Returning to logic design after decades of absence,  I want to present an Or-gate function at the Keyboard socket of the Personal computor (IBM Design but one of 100's of manufacturers).      Easy, i thought  = just insert a diode type 1n916 and the Or function can be realised  -- you might think.

But it doesn't work and scoping it, I am 90 % sure its because such an Or-gate needs a pull down resistor.

However, I do not know the exact type of logic used, inside  this now highly compacted "Black Box" called a PC !

I was just going to inset a 100,000 ohm resistor,  when i realised if i got that wrong, I could blow up the front end of which ever PC I was using !

and unlike our early days in Computing (the noble 50's and 60's) when we would actually take equipement to pieces,  find the blown transistor and replace it,  I would have to throw my computor away or only drive it from the Mouse ! ? !

So all i can be sure of, is that my resistor would go to deck, that is Nought volts,  but reading your locid discussions, I estimate someone could given me an "exact" figure for such a resistor  and save me from ruining several fully working computors..