Part Number: SN74LVC16245A
Tool/software:
Hi all,
When using 8 bits each, I think each group can operate independently.
If I don't assert both 1OE and 2OE, I can't use 8 bits.
I can access 16 bits without any problem.
Also, a similar circuit configuration on a separate board works independently for each 8 bits without any problem.
1) Have there been similar cases in the past?
2) Is it possible that the OE pin is short circuited? Is it possible that it is in a state like this?
3) Is it possible that the peripheral circuit is affected?
We are aware that pull-up resistor connection is recommended.
However, we think that pull-up is unlikely to be the direct cause because it is stable when the power is turned on.
Best Regards,
Ryusuke