Part Number: SN74AVC4T245
Tool/software:
Hey, im using two sn74avc4t245 for uart debug interface of a processor.
I connect them the following way:

So X_VCCA and Y_VCCA comes from the card and VCCB comes from the connector (for example plugging ftdi cable).
I dont have for now extra pin on the connect to divide vcc_b between both level shifters so i shorted them
My question is what happens for the following situations:
1. Device X and Y is off so X_VCCA and Y_VCCA is off and i plug ftdi cable and give VCC_B? Or only one device is on while VCC_B is on for both?
2. Device X is On and i plug ftdi cable without applying VCC_B while keeping OE high? What if OE will be low?
3. I can maybe somehow make room for extra pin to divide VCC_B, but i prefer not to to save one pin on the connector (if not possible i will make the change)
Thanks,
Michael