TXV0108-Q1: TXV0108-Q1

Part Number: TXV0108-Q1
Other Parts Discussed in Thread: TXV0108, TXV0106-Q1, TXB0304

Tool/software:

Hi, 

I need help with selecting appropriate level shifter.
I need to use it for SDHC, so I need translations from 3.3 to 1.8 and vice versa.

- The output rise/fall times should not exceed 3ns

- Frequency of operation: 10MHz

- Explicit direction control pin

- The IOs of level shifter should support pull-up/pull-down resisters of 20kohm and higher. Since the TLA probe has 20kohm internal pull-down.

Is TXV0108-Q1 right choice for this?