This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCT245: please recommend a device which is P2P with SN74HCT245DWR and supports bus hold feature

Part Number: SN74HCT245


Tool/software:

Hi,

Pls kindly help recommend a device which is P2P with SN74HCT245DWR (SOIC (DW) | 20 ) and supports following features. SN74HCT245DWR was already designed by customer.

  1. with Bus hold feature.
  2. Vcc=3.3V

I find that SN74ABTH245DW has bus hold feature but can't support VCC=3.3V.