This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All
I used FLUKE 187 multimeter measure the ICC is 1mA, compare the datasheet 40uA is differences
Test condition
VCC=/1CLR=/2CLR=5V
/1PRE=/2PRE=GND=0V
How do I measure max ICC below 40uA?
All of the device input pins, including J & /K need to be at either VCC or GND to get the specified ICC value. Refer to the following TI application report.