Can the SN75LVDT1422 SERDES operate with a burst clock (see customer inquiry, below)?
Will the PLL achieve a faster lock if the clock burst off ime is under the typical PLL lock time?
Customer's Application
GPN: SN75LVDT1422
LGC, Semiconductor Technical Support, www-k.ext.ti.com, SN75LVDT1422
Question about SN75LVDT1422 Hello, I am considering the use of the 1422 in a new design. One of the questions that I have about using this part is how it will respond to my clock signal. In this application, my clock comes in bursts. I am concerned that with a 'gated' clock, that this part may not work. Can you confirm or deny my suspicions? Clock rates are on the order of 100 kHz to 200 kHz depending on the application. Dead times between clock bursts are on the order of 82 uS to 2.9 mS.
Thanks,
Phil