Hi,
I would like to use SN74LVC2G17 to translate logic levels from 2.8V CMOS to 3.3V. The buffer operational voltage is 3.3V. Vt+ (positiv-going input threshold voltage) is the most crucial parameter for my application. The datasheet give Vt+min and Vt+max for 3.0V VCC. I did not find that information in IBIS file too. Could you tell me Vt+ voltage level for 3.3V VCC?