Other Parts Discussed in Thread: TMS320F28335, TXS0108E, OMAP3530, TXB0108, TXS0104E, SN74AVC8T245
Hey,
I'm trying to interface a OMAP 3530 over serial with a Delfino TMS320F28335.
The OMAP3530 is in the form of a Gumstix COM with the summit break outboard, and I am using the Spectrum Digital ezDSPf28335 kit. The OMAP processor operates on 1.8V and the Delfino operates on 3.3V logic. I was attempting to use a TXB0108 logic level shifter to shift the SCI (serial) channels and a TXS0108e chip to shift I2C and SPI channels.
Right now I'm only really concerned with making the TXB0108 work. When I power the Delfino and the Gumstix (OMAP) separately and scope the outputs, I get nice clean digital signals. When I hook up the two devices with a TXB0108 between them, I get high frequency high amplitude noise on both the driving and receiving lines. I would be happy to post a schematic of my circuit, but I was hoping that someone could tell me if this is a correct way to handle the level conversions.
If someone is willing to take the time to help me figure this out, I'd be happy to write it up so Gumstix and Beagleboard users don't have to go through the guessing games that I did when I designed my board.
Thanks for the help!
Daniel McKenna