This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G07: Design Questions

Part Number: SN74LVC2G07

Tool/software:

Hi expert,

I have a few questions about SN74LVC2G07.

What leads to recommended output drive current to be 4mA max when supplied by 1.65V?

Will VOL rise slightly if it is more than that, say around 8mA? If you stay under 50mA are you free from damage?

Do you have any footprint compatible parts with similar behavior with a stronger drive strength, say 15 mA when supplied by 1.8V and tolerate up to 150mA continuous in fault conditions?

I am using the smallest package.

Thank you!

McKenna