This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4050B: input, output, Vcc convertion

Part Number: CD4050B
Other Parts Discussed in Thread: CD4504B, CD40109B, TLV1811

Hi,

Our customer want to know if the input is 2.5V, VCC is 15V ,can the output reach 15V? I couldn't find this information in datasheet.

VCC=15V, Vin=2.5V, Vout=15V, that is customer's design goal, if CD4050B can not meet, please recommend other devices, thanks!

 

  • The input signal is too low for the specified VIH.

    Level shifters like the CD40109B or CD4504B are not specified for voltages below 5 V.

    Use a comparator like the TLV1811 that compares the input signal against a reference voltage of about 1.25 V.