This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV00A: Part Number Date Code / Suffix Clarification

Part Number: SN74LV00A
Other Parts Discussed in Thread: SN74AHC00

What's up TI. 

This NAND gate is used to invert a 28 MHz bit clock driving the pixel grid on a 8" TFT LCD.  We find that newer variants (2025) of this part have slightly more vertical edges than 2023 variants of the same part.  Because of this the 2025 variant produces a high frequency harmonic at 489.7 MHz that causes us to fail EMC compliance.  The 2023 version of this part does not produce this harmonic at all.  I have attached macroscope photos of both.  Can you please rationalize the differences between these parts?

LV00A 2023.jpg

LV00A 2025.jpg