Part Number: CD4047B
I have been working with the CD4047 for well over 30 years. I have just encountered a very strange anomaly. I was utilizing a series of three 4047s in a progressive timing sequence. I was using the monostable mode. The first chip was configured Positive-Edge Trigger. The following two stages were configured Negative-Edge Trigger. The circuit was functioning as expected. I then modified the timing components and added a new front end timing pulse. The new front end was added to the design to facilitate external triggering of the timers. I added a jumper to be able to switch between the onboard oscillator used for calibration. The nature of the anomaly:
Since the above-mentioned modifications, the first one-shot is functioning normally, the next one-shot is outputting a steady high.
I consulted Grok seeking troubleshooting advice. It noted that the monostable Negative-Edge Trigger had a tendency to be temperamental. I implemented the suggestions but have been unable to get the oneshot to function.
The circuit is built on a Radio Shack 276-168B Breadboard PCB.
I have tried replacing the 4047 with different build dates chips with the same result.
I have verified that the wiring is correct numerous times.
I removed the third chip to see if that was causing the issue. No change.
I added a CD40106 between the first and second oneshot. No change.
This is the as-built schematic.