Part Number: TMUX4053
hi,
is there any UVLO for the TMUX4053 ?
what would happen if VDD is or drops to 4V ?
thanks
Vincenzo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMUX4053
hi,
is there any UVLO for the TMUX4053 ?
what would happen if VDD is or drops to 4V ?
thanks
Vincenzo
Hello Vincenzo,
No, our parts do not have UVLO.
If VDD drops to 4V the device will probably will not be fully turned on the and you won't be able to pass signals through.
Though, this is a theory since I can't guarantee device operation below rated specs.
I can recommend to implement the SN74LV4053A instead, if the customer needs to operate at lower voltages.
It is p2p with the TMUX4053.
Thanks,
Nir