Part Number: TXB0108
Other Parts Discussed in Thread: TXB0604, TXS0108E
Hi,
We have used TXB0108 bidirectional buffer in 1.8V logic (Vcca & Vccb). In the datasheet for Vcca & Vccb = 1.8V, the maximum data rate supported is 52Mbps. Our SPI clock is 50MHz and at the output side of this buffer we are receiving only 25MHz clock output. SPI clock at 50MHZ won't work with this part? What about TXS0108? We cannot reduce SPI clock as the clock speed is fixed for the application.
We have specific reason for 1.8V on both Vcca & Vccb. Bidirectional buffer is required because we may switch to QSPI mode.
Need support from TI as soon as possible.
Regards
Hafiz Haja