This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXU0104: Logic level lower limit

Part Number: TXU0104
Other Parts Discussed in Thread: TLV9034, SN74AXC4T245

Hello,

We would like to use the TXU0104 to interface with an IC with 1V logic levels (IC provides 1V input to TXU0104 and level shifts it to 3.3V). The positive-going threshold voltage suggests that 1V inputs may work, though VCCA is only rated down to 1.1V. Would the TXU0104 work with VCCA=input logic level=1V (as opposed to VCCA=1.1V, logic=1V, for example)?

Thanks.