This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G240: Schematic Review

Part Number: SN74LVC1G240

Dear Team,

I am controlling two MUX's using SN74LVC1G240. During power on all the MUX's are disabled.

When 8:1 MUX is enabled the 4:1 MUX should be disabled.

For implementing this logic I used SN74LVC1G240 for controlling the EN pin of 4:1MUX. The main enable signal(WE_MUX_EN) will directly come to 8:1 MUX EN and OE(Active Low) of the SN74LVC1G240.

When "WE_MUX_EN" is High 8:1 MUX is enabled and when it is low 4:1 MUX is enabled. Please see my circuit below. May I know this is correct or not.

image.png