Part Number: SN74LVC8T245
Hello E2E Experts,
Please see the circuit below, in regards, to how we are using the SN74LVC8T245. Data is input at B and output at A. You recommend powering up the input (VB) before powering up the output (VA). We are doing the opposite. The power sequencing on our board is such that VA (5V) comes up before VB (2.5V). 2.5V is generated from 5V. The OE enable is referenced to VA (5V). The pulldown (R405) has been removed. We now have a 10K pullup on the OE to VA (5V) which is not reflected in the circuit below. What is the state of the outputs at A while the VB (2.5V) comes up? Are the outputs at A guaranteed tristated (high impedance) state until the VB reaches active level 1.65V, which is the minimum VCC level, even though VA is already 5V?