Part Number: SN74LVC595A-Q1
Hi,
We are thinking of using the SN74LVC595A-Q1 device. Due to the large number of devices on 1 board, we like to have an accurate current consumption of 1x SN74LVC595A-Q1 device, to calculate the totale board consumption.
We are using an SRCLK of ~35MHz. All inputs will get Vinh>=3.0V. The max ambiant temperature will 60 degrees celsius. All outputs of the device will sink current from a different power supply (not the 3.3V VCC).
What would the max current consumption be for one device?
Best regards,
Ben