This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74GTL2003: level translation solution for data buses

Part Number: SN74GTL2003
Other Parts Discussed in Thread: TXS0108E, SN74CB3T3245

Hello,

I'm looking for a voltage level translation solution for an 8-bit data bus between a 5V processor and a 3.3V FPGA.

The bus is a 3-state bus managed by the processor.

I had identified the SN74GTL2003, but I've noticed that it requires low-value pull-up resistors, which can lead to significant power consumption in some cases.

I've also seen the TXS0108E; would it be suitable? It doesn't seem to require pull-up resistors.

Would a solution using the SN74CB3T3245 be appropriate?

Thank you in advance.