Hi,
I am using level shifters in 2.5V controller and 3.3V IO application. i am using the part SN74CB3T16210.
could some one clarify me if each A port or pin can be in any direction or all the A ports are to be on single direction?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using level shifters in 2.5V controller and 3.3V IO application. i am using the part SN74CB3T16210.
could some one clarify me if each A port or pin can be in any direction or all the A ports are to be on single direction?
thanks
Hello,Prasanthi
For SN74CB3T16210, yes, Each A port or pin can be in any dirction if the OE is enable. any further concern, please let me know.
BR
junjie
Hello,
Sorry for jumping into the thread, but I think this is the correct place to chip-in.
I am also using the same IC (SN74CB3T16210) for my application. In my case the voltage is not translated from 2.5 to 3.3 volts. Is it that, it only works for translating voltage from HIGH to LOW?
Thanks in Advance.
Hi,
The datasheet actually say " if the input applied is in range VCC-1V to 5.5V, the output voltage will approximate to VCC". So just look into the voltage level you are applying as input and also the VCC voltage you are using. can i know what is the vcc you are applying in your case?
Thanks