Part Number: SN74LVC2G240
Hi,
For the SN74LVC2G240 component, in the YZP package, there are two different pinout definitions shown in the datasheets. Which one is correct?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC2G240
Hi,
For the SN74LVC2G240 component, in the YZP package, there are two different pinout definitions shown in the datasheets. Which one is correct?
Thanks!
Hi, I saw the one you sent and this one from the mechanical drawing:

in one leg 2 is near one and in the other leg 1 is near 1, which is correct?
The drawing you are showing is the mechanical drawing, it shows pins "A1" and "A2" not "1" and "2" because this is a BGA package. A1 is equivalent to "1" in the front page drawing.