This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G06



Regarding the subject line part, I noticed in the datasheet that the part specifies the low level output current and voltage in the datasheet as shown below:

 


 

The datasheet does not specify the high level output current and voltage. On the main TI webpage for the part, the IOH is -32mA.

Does this follow based on the currents in the table above that -32mA is for Vcc=4.5V? -24mA for Vcc = 3V? etc...

Regards,

Jeramie