Part Number: CD74ACT245
Hello,
The CD74ACT245 datasheet specifies +/-100mA Vcc or GND current maximum, which increases to 200mA when all 8 outputs are sourcing or sinking current.
It appears that this is to be interpreted as a DC current - is there a higher limit for Vcc or GND current for short (<50ns) transient conditions?
If no higher transient rating can be provided, what is the risk of exceeding this current rating for very short durations?
Thank you,
Nick