Part Number: SN74LXC8T245
Other Parts Discussed in Thread: SN74AXC8T245
Dear TI forum, I'm trying to undestand what would be the minimum (worst case) and typical bandwidth of the SN74LXC8T245 when both Vcca and Vccb are equal to 3.3 V. Using this FAQ as a reference and the maximum t_pd of 9 ns (from 6.10 Switching Characteristics) I get an estimated ~111 Mbs worst case. Is that correct? Conversely the in best case of t_pd == 3 ns I could expect 333 Mbps. Is that true?