Part Number: LSF0204
Kindly help share the following values:
- VOH, VOL, VIH, and VIL values for LSF0204RUT
- VIH and VIL values for TCAL9539RTW
- VIH and VIL values for the EN pin of TPS2492PW
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. The LSF does not have digital buffers. For input voltages below Vref_A, it works as an analog switch. For input voltages above Vref_A, the switch is off, and the output voltage is determined by the pull-up resistor.
2. These values are specified in the recommended operating conditions.
3. See the VUVEN_H specification; VIL = 1.31 V − 120 mV = 1.19 V; VIH = 1.39 V.