Part Number: SN74AVC2T245
I connected the DIR pin of the SN74AVC2T245 directly to VCCB (+3.3V) instead of VCCA (+1.8V).
It seems to have overvoltage protection, but will this cause any problems?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AVC2T245
I connected the DIR pin of the SN74AVC2T245 directly to VCCB (+3.3V) instead of VCCA (+1.8V).
It seems to have overvoltage protection, but will this cause any problems?
Hello Yuki,
Yes, you can connect 3.3V to DIR when VCCA is 1.8V.
Regards,
Josh