Part Number: TXS0108E
Other Parts Discussed in Thread: TXU0304
Hi there!
I'm analyzing the TXS0108ERGY to use in a project that needs level adaptation from 5V to 3,6V. I've seen in the datasheet this device has internal pull-ups in all the lines, connected to their respective supply levels and I have some doubts regarding this features. Is it recommended to use this resistors to set the default states of signals that need a specific value, such as enable pins of another devices? For example, If am driving a RESET signal, that needs a pull-up, can this internal pull-up used instead of placing an external one for time constrained applications?
And... in case I place an external pull-up resistor, the equivalent resistor should be considered to be the parallel between the external resistor and the internal one, depending if the signal is driving high or low (as in section 7.3.5 of datahseet indicates the Rpua and Rpub changes depending if the signal is high or low).
And 2... what about if I need to place an external pull-down in a signal? Can this device handle that situation, or do I need another level translator without the internal pull-up to handle that default pull-down pins?
Thanks!!