Part Number: LSF0204
Dear Team,
we would like to use LSF0204 for:
-> I2C (400kHz) translation from 3.3V ( Master) to 1.8V (slave)
-> Gpio translation from 3.3V to 1.8V
1) We only use 3 channelc, can we connect booth A and B Side of fourth channel to GND?
2) We will connect Vref_B to 3.3V and Vref_A to 1.8V and have 100nF on Vref_a and 100nF on Vref_B. is it ok?
3) We will connect EN to Vref_A -> 1.8V as the 1.8V is generated with LDO from 3.3V is it ok?
4) How to size the pull-up for the I2C 400kHz ->
SDA(SCL on the A site

For the B site ( 3.3V) Rpullup 1kOhm?
For the A site (1.8V) Rpullup 464Ohm?
Or can we also have larger resistors?
5) Regarding the reistor for the GPIO we also need pull-ups , how to size them?
the GPIO input is as below

Best Regards,
d.