Part Number: INTERCONNECT-STUDIO
Other Parts Discussed in Thread: TPLD2001
Hi everyone,
I'm trying to validate a design based on the TPLD2001 using the Interconnect-Studio simulation tool. I encounter the following error when I use an analog comparator (acmp). Is there any workaround, did I do a configuration mistake or might this be a bug?
Best regards
Tristan
Log:
Simulation Failed: SpiceDataFile: file not initialized, simulation results are incorrect
warning, can't find model 'hyst18' from line
ahys18_acmp0 hyst_acmp0_in a_hyst18_acmp0 hyst18
warning, can't find model 'hyst25' from line
ahys25_acmp0 hyst_acmp0_in a_hyst25_acmp0 hyst25
warning, can't find model 'hyst33' from line
ahys33_acmp0 hyst_acmp0_in a_hyst33_acmp0 hyst33
warning, can't find model 'hyst50' from line
ahys50_acmp0 hyst_acmp0_in a_hyst50_acmp0 hyst50
Error on line 0 or its substitute:
a.x_dynamic0.ahys18_acmp0 x_dynamic0.hyst_acmp0_in x_dynamic0.a_hyst18_acmp0 hyst18
MIF-ERROR - unable to find definition of model hyst18
Simulation interrupted due to error!
Note: No ".plot", ".print", or ".fourier" lines; no simulations run
Note: No compatibility mode selected!
Circuit: *// transient simulation //*
Note: No compatibility mode selected!