This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G04: SN74LVC2G04YZPR About the pin assignment

Part Number: SN74LVC2G04

Could you please provide the correspondence between the package outline ball positions (A1, A2, B1, B2, C1, C2) and the pin numbers (pin names) for the SN74LVC2G04YZPR?
  • Section 5 shows the pin names and pin numbers, in bottom view:

    The YZP0006 package outline shows the balls, also in bottom view:

    (The example board layout and stencil design show top views.)

    So:

    pin name pin number ball position
    1A 1 A-1
    GND 2 B-1
    2A 3 C-1
    2Y 4 C-2
    VCC 5 B-2
    1Y 6 A-2