Part Number: TXS02612
Other Parts Discussed in Thread: TMUX1574, AM6442, TXS0206A
Does TXS02612 support SD card High-Speed Mode?
When VCCA = 3.3 V and VCCB = 3.3 V:
The propagation delay (tPD) of clock from controller to SD card (CLKA to CLKB) is 3.5 ns (max).
The propagation delay (tPD) of data from SD card to controller (DATB to DATA) is 3 ns (max).
For SD Card High-Speed Mode:
The Output Delay Time during Data Transfer Mode (tODLY) is 14 ns (max).
The total of these delays is 20.5 ns, which exceeds the 20 ns clock period of High-Speed Mode (50 MHz).
The TXS02612 is unlikely to support SD card High-Speed Mode.
Best regards,
Daisuke