Part Number: SN74LVC06A
I need to put capacitor on the buffer output to delay signal.What can be max . capacitor value that will not damage the buffer when oitput switched to low and capacitor is discharged through the buffer?
Part Number: SN74LVC06A
I need to put capacitor on the buffer output to delay signal.What can be max . capacitor value that will not damage the buffer when oitput switched to low and capacitor is discharged through the buffer?
Hi Yigal,
Clemens is correct! For more information, please refer to the following FAQ: (+) [FAQ] What is the maximum capacitive load that a logic device can drive? - Logic forum - Logic - TI E2E support forums
Regards,
Kollin