Part Number: TXB0104
Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204, SN74AXC4T774
Hello.
I have a question regarding the use of the TXB0104.
Side A is connected to a component, while Side B is open. (Figure 1)
When power is applied, as shown in Figure 2, the pull-up resistor connected to pin 2 operates and goes high. This causes pin 9 of the B side to go high, allowing the component connected to Side A to operate normally. However, occasionally, as shown in Figure 3, pin 2 outputs a low signal before the pull-up resistor connected to pin 2 operates, causing pin 2 to go low and the component connected to Side A to stop functioning.
Is there any reason why pin 2 of Side A outputs a low signal when Side B is open?
Please let me know if there is a replacement part available to resolve this issue. (Pin 2 of Side A must go high when power is applied, and it only needs to operate once upon power application.)