This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hspice simulation of a board

Hi,

       I am using LVC1G04 HSpice model in my board - simulation. The library (LVC1G04) has to be called more than one number of times (as driver and receiver, connected with some interconnect traces). Can anyone please help whether it is possible to call more than one instance of a single component library (when it is encrypted).

Regards

  • Hw47343 said:

    Hi,

           I am using LVC1G04 HSpice model in my board - simulation. The library (LVC1G04) has to be called more than one number of times (as driver and receiver, connected with some interconnect traces). Can anyone please help whether it is possible to call more than one instance of a single component library (when it is encrypted).

    Regards

    Hi Chris,

                            Please delete this post. It works now.

    Thanks.

  • Hi,

    We are closing this post due to inactivity. Please feel free to post again if you have any further questions.

    Regards,
    Aaron Goodson